:MEASure:EYE:PAM:EWIDth:DEFine:EOPening:PROBability

Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
PAM4/6/8

Command Syntax

EYE:PAM:EWIDth:DEFine:EOPening:PROBability <probability>

<probability> is a double.

Query Syntax

EYE:PAM:EWIDth:DEFine:EOPening:PROBability?

Description

Sets the eye-opening probability for the Eye Widths measurement. The entered measurement-hit probability establishes the contour of an eye's opening. The probablility can be set from 1 x 10–1 to 1 x 10–9. The default probability is 1 x 10–2. No extrapolation is used to determine Eye Widths at a specified probability. To select to use a probability target instead of zero data hits, use the :DEFine:EOPening parent command.

Requires FlexDCA revision A.04.50 and above.