:MEASure:EYE:PAM:EWIDth:DEFine:EOPening:RNSValue:LEVel

Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
NRZ
PAM4/6/8

Command Syntax

:MEASure:EYE:PAM:EWIDth:DEFine:EOPening:RNSValue:LEVel{0|1|2|3} <random_noise>

<random_noise> is a double.

Query Syntax

:MEASure:EYE:PAM:EWIDth:DEFine:EOPening:RNSValue?

Description

For a PAM4 Eye Width measurement, sets the value of RN used for RN stabilization for the selected eye level. PAM4 signals have four possible levels: 0, 1, 2, and 3. NRZ signals has two possible levels: 0 and 1. There are actually four commands, one for each eye level on the signal.

  • :MEASure:EYE:PAM:EWIDth:DEFine:EOPening:RNSValue:LEVel3 (for PAM4 only)
  • :MEASure:EYE:PAM:EWIDth:DEFine:EOPening:RNSValue:LEVel2 (for PAM4 only)
  • :MEASure:EYE:PAM:EWIDth:DEFine:EOPening:RNSValue:LEVel1 (for NRZ and PAM4)
  • :MEASure:EYE:PAM:EWIDth:DEFine:EOPening:RNSValue:LEVel0 (for NRZ and PAM4)

To measure the RN, switch the N1000A to Jitter Mode and measure the RN while using a signal that has a short pattern. Or, measure the RN using a separate instrument. Use the :MEASure:EYE:PAM:EHeight:DEFine:EOPening:RNSTabilize command to turn on or off the use of RN stabilization.

Command Description
RNSValue:LEVel3 Applies to level 3.
RNSValue:LEVel2 Applies to level 2.
RNSValue:LEVel1 Applies to level 1.
RNSValue:LEVel0 Applies to level 0.

Linked RN Stabilization (On / Off) Commands

The following commands are equivalent. Turn one setting on and both are turned on.

Linked RN Value Commands

The RNSValue:LEVel commands for the same eye level for Eye Width and Eye Height measurements are equivalent. Use one of a commands to enter a value for one level on a measurement and it is changed on both measurements. For example, enter the level two value for an Eye Height measurement and the level two value is also entered for for an Eye Width measurement.

Requires FlexDCA revision A.05.30 and above.