:MEASure:EYE:PAM:VECLosure:DEFine:EOPening

Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
NRZ
PAM4/6/8

Command Syntax

:MEASure:EYE:PAM:VECLosure:DEFine:EOPening {ZHITs | PROBability}

Query Syntax

:MEASure:EYE:PAM:VECLosure:DEFine:EOPening?

Query Response

{ZHIT | PROB}

Description

Selects the Eye Opening Definition for the :MEASure:EYE:PAM:VEClosure measurement to be either the Zero Hits (ZHIT) or At Probability (PROBability). The default Eye Opening Probability is 10–6. When PROBability is specified, use the following child commands to define the probability:

To specify the measurement Reference, use the :MEASure:EYE:PAM:VEClosure:REFerence command.

Requires FlexDCA revision A.06.60 and above.