:MEASure:EYE:PAM:VECLosure:DEFine:EOPening:PROBability

Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
PAM4/6/8

Command Syntax

:MEASure:EYE:PAM:VECLosure:DEFine:EOPening:PROBability <double>

Where <double> is a probability.

Query Syntax

:MEASure:EYE:PAM:VECLosure:DEFine:EOPening:PROBability?

Description

Enters a value of Eye Opening Probability to be used when the VEC measurement's Eye Opening Definition is set to At Probability (:MEASure:EYE:PAM:VECLosure:DEFine:EOPening).

Requires FlexDCA revision A.06.60 and above.