:MEASure:EYE:PAM:VECLosure:DEFine:EOPening:RNSValue:LEVel

Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
NRZ
PAM4/6/8

Command Syntax

:MEASure:EYE:PAM:VECLosure:DEFine:EOPening:RNSValue:LEVel <double>

Where <double> is an RN value in volts.

Query Syntax

:MEASure:EYE:PAM:VECLosure:DEFine:EOPening:RNSValue:LEVel?

Description

Enters a fixed RN value for the specified level. This value is applied to the VEC measurement when Fixed RN has been selected with the :MEASure:EYE:PAM:VECLosure:DEFine:EOPening:RNSTabilize command. Select the desired level by appending a 0, 1, 2, or 3 to identify the level as shown in the following picture. The actual RN is sent as a command argument. For example, to specify an RN of 5 μs for level 2, send this command:

:MEASure:EYE:PAM:VECLosure:DEFine:EOPening:RNSValue:LEVel2 5E-6;

Eye and Level ID Numbers for PAM4 Signal

If VEC is measured on an NRZ signal, there are fewer Fixed RN settings as required for only two levels. This requires only two fixed RN values (levels 0 and 1) instead of four (levels 0, 1, 2, 3).

Requires FlexDCA revision A.06.60 and above.