:MEASure:EYE:PAM:VECLosure:DEFine:EOPening:RNSTabilize

Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
PAM4/6/8

Command Syntax

:MEASure:EYE:PAM:VECLosure:DEFine:EOPening:RNSTabilize {ON | OFF | 1 | 0}

Query Syntax

:MEASure:EYE:PAM:VECLosure:DEFine:EOPening:RNSTabilize?

Description

Turns RN stabilization on or off. RN stabilization can be selected when the VEC measurement's Eye Opening Definition is set to At Probability (:MEASure:EYE:PAM:VECLosure:DEFine:EOPening). To enter the RN values to use when RN stabilization is on, use the :MEASure:EYE:PAM:VECLosure:DEFine:EOPening:RNSValue:LEVel command.

Requires FlexDCA revision A.06.60 and above.