:MEASure:EYE:TTIMe
Command Syntax
:MEASure:EYE:TTIMe
Query Syntax
:MEASure:EYE:TTIMe?
Description
The Eye/Mask mode IEEE 802.3cd PAM Transition Time measurement measures the transition time on PAM4/6/8 waveforms. The query form of the command returns the selected transition time measured. Use the :MEASure:EYE:TTIMe:TRANsition child command to select from three available transition time measurements:
- Slowest edge
- Average rising edge
- Average falling edge
By default, measurements are made on the following edges:
- Rising edges: A run of at least 5 level zeros, leading Consecutive Identical Digits (CIDs), and 6 level threes, lagging CIDs.
- Falling edge: A run of at least 5 level threes, leading Consecutive Identical Digits (CIDs) and 6 level zeros, lagging CIDs
The transition time is measured as the waveform's edge transitions through the 20% to 80% amplitude levels between the average level zero and average level three. The average level amplitudes are measured using the same algorithm as is used for the Outer OMA measurement (:MEASure:EYE:OOMA).
You can change the default minimum leading and lagging CIDs with these commands:
Before making this measurement, apply a System Impulse Response Correction (SIRC) data digital filter. Use the :CHANnel:SIRC and :CHANnel:SIRC:FRATe commands.
Requires FlexDCA revision A.06.00 and above.
Measurement Identification
Avoid subtle programming errors! To ensure that the correct measurement is installed or queried, always explicitly identify a measurement when installing a measurement or querying a measured value, status, or detail. To identify a measurement, specify the measurement's source waveform (:SOURce child command). With some measurements, you may also need to specify other identifying values. Generally, when selecting a measurement using FlexDCA's GUI, if a dialog appears prompting you to select values, you should explicitly specify these values when remotely identifying the measurement. More information.
For example, to return the status of the measurement, :MEASure:EYE:TTIMe
flex.write(':MEASure:EYE:TTIMe:SOURce CHAN1A')
if flex.query(':MEASure:EYE:TTIMe:STATus?') == 'CORR';
measurement = flex.query(':MEASure:EYE:TTIMe?')
else:
details = flex.query(':MEASure:EYE:TTIMe:STATus:DETails?')
reason = flex.query(':MEASure:EYE:TTIMe:STATus:REASon?')
Child commands for measurement identification:
:MEASure:EYE:TTIMe:SOURce:MEASure:EYE:TTIMe:TRANsition
Measurement Ready?
To confirm that the measurement is ready to read, you can query the measurement's status:
if ('CORR' in Flex.query(':MEASure:EYE:TTIMe:STATus?')):
measurement = Flex.query(':MEASure:EYE:TTIMe?')
If averaging is turned on (:ACQuire:AVERaging), you can also confirm if the measurement result is ready by comparing the number of specified averages (:ACQuire:ECOunt?) versus the number of measurement sweeps that have occurred (:MEASure:EYE:TTIMe:COUNt?). The technique uses the :COUNt? common measurement query. For example,
if (Flex.query(':MEASure:EYE:TTIMe:COUNt?') >= Flex.query(':ACQuire:ECOUNt?')):
measurement = Flex.query(':MEASure:EYE:TTIMe?')
You can also use an acquisition limit lest to test that a number of waveform samples, or pattern acquisitions have completed before returning a measurement. Refer to the :LTESt:ACQuire:CTYPe command.
Common Measurement Child Queries
This command supports the use of the following common measurement queries: :LOCation?, :COUNt?, :MAXimum?, :MINimum?, :MEAN?, and :SDEViation?.