:MEASure:PAM:TTIMe:CIDigits:LAGGing
Instrument mode:
Eye
Waveform type:
NRZ
PAM
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:MEASure:PAM:TTIMe:CIDigits:LAGGing <integer>
Where <integer> is a integer from 1 through 15.
Query Syntax
:MEASure:PAM:TTIMe:CIDigits:LAGGing?
Query Response
<integer>
Description
For the PAM4 Transition Time measurement (:MEASure:EYE:TTIMe) in Eye/Mask mode, specifies the minimum number of lagging Consecutive Identical Digits (CIDs) required when measuring waveform transition times. To set the minimum number of leading CIDs, use the :MEASure:PAM:TTIMe:CIDigits:LEADing.
The default value is 6. The minimum value is 1. The maximum value is 15.
Requires FlexDCA revision A.06.50 and above.