:MEASure:EYE:USER:ABBReviation?
Meas. mode:
Eye
Waveform type:
NRZ
PAM4
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:MEASure:EYE:USER{1:8}:ABBReviation?
Description
For the selected Eye mode user measurement, returns the abbreviated test name. If an XML file was used to define the test, the abbreviated test name is specified in the file's XML <Abbreviation> tag. If this tag is missing, or empty, or if the user measurement was defined directly from a Matlab (*.m) or Python (*.py) file, the abbreviation is derived from the XML, Matlab, or Python filename. The abbreviation string is shown in the displayed Measurement results table and is limited in length to 15 characters.
Use the :MEASure:EYE:USER parent command to turn on the measurement and return the measured value.
Requires FlexDCA revision A.05.00 and above.