:MEASure:EYE:USER:CFILe:RELoad
Meas. mode:
Eye
Waveform type:
NRZ
PAM4
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:MEASure:EYE:USER{1:8}:CFILe:RELoad
Description
Reloads the XML configuration file for the selected user-defined measurement.
Use the :MEASure:EYE:USER parent command to turn on the measurement and return the measured value.
Requires FlexDCA revision A.05.00 and above.