:MEASure:EYE:USER:COMMents?
Meas. mode:
Eye
Waveform type:
NRZ
PAM4
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:MEASure:EYE:USER{1:8}:COMMents?
Description
Returns the comment string for the selected user measurement. The comment string is defined in the measurement's XML definition file using the <Comments> tag. The comment string is limited in length to 512 characters.
Use the :MEASure:EYE:USER parent command to turn on the measurement and return the measured value.
Requires FlexDCA revision A.05.00 and above.