:MEASure:EYE:USER:CFILe:CLEar
Meas. mode:
Eye
Waveform type:
NRZ
PAM4
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:MEASure:EYE:USER{1:8}:CFILe:CLEar
Description
Removes an existing configuration file for a user measurement. This removes the measurement from Eye mode's User toolbar. A user measurement is created using the :MEASure:EYE:USER:CFILe parent command.
Use the :MEASure:EYE:USER parent command to turn on the measurement and return the measured value.
Requires FlexDCA revision A.05.00 and above.