:MEASure:EYE:USER:CFLoaded?
Meas. mode:
Eye
Waveform type:
NRZ
PAM4
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:MEASure:EYE:USER{1:8}:CFLoaded?
Query Response
{1 | 0}
Description
Queries the existence of the specified user measurement. Returns a one if the measurement is defined and a zero it the measurement has not been setup.
Use the :MEASure:EYE:USER parent command to turn on the measurement and return the measured value.
Requires FlexDCA revision A.05.00 and above.