:MEASure:REGions:ALIGn
Meas. mode:
Scope
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:MEASure:REGions:ALIGn
Description
Automatically distributes all displayed regions evenly across the entire display. No gap is placed between the regions.
Requires FlexDCA revision A.01.70 and above.
Measurement regions are only available in Oscilloscope and TDR modes.
The Jitterp-p and Jitterrms measurements can not be made on a measurement region.
Example Command Sequence
:SYSTem:MODE OSCilloscope :MEASure:REGions:STATe ON :MEASure:REGions:ALIGn