:MEASure:REGions:REGion:X
Meas. mode:
Scope
TDR
Flex Apps:
FlexDCA
Command Syntax
:MEASure:REGions:REGion{1:8}:X{1:2} <time>
<time> is an double.
Query Syntax
:MEASure:REGions:REGion{1:8}:X{1:2}?
Description
Defines a specific measurement region's left and right boundaries (x-axis). The boundaries of up to eight regions can be defined, but you must first set the number of regions available using the :MEASure:REGions:COUNt command. To turn on all defined regions, use :MEASure:REGions:STATe command.
Requires FlexDCA revision A.01.70 and above.
Measurement regions are only available in Oscilloscope and TDR modes.
Example Command Sequence
:SYSTem:MODE OSCilloscope :MEASure:REGions:COUNt 1 :MEASure:REGions:REGion1:X1 40E-12 :MEASure:REGions:REGion1:X2 100E-12 :MEASure:REGions:STATe ON