Measurement Region Setup

Meas. mode:
Scope
TDR
Flex Apps:
FlexDCA

The measurement region commands define a restricted range of input data that is used when performing Oscilloscope Mode or TDR/TDT Mode measurements. Up to eight regions can be defined using x-axis boundaries. Measurement regions can be applied only to Oscilloscope-Mode measurements. The only Oscilloscope-mode measurements that can not be applied to a measurement region are Jitter rms and Jitter p-p.