:MEASure:REGions:COUNt
Meas. mode:
Scope
TDR
Flex Apps:
FlexDCA
Command Syntax
:MEASure:REGions:COUNt <count>
<count> is an integer from 1 to 8.
Query Syntax
:MEASure:REGions:COUNt?
Description
Established the maximum number of available measurement regions for definition, enabling, and use. Up to eight regions can be defined. The default quantity is two. To define a specific region's left and right boundaries (x-axis), use the :MEASure:REGions:REGion{1:8}:X command. To turn on all defined regions, use :MEASure:REGions:STATe command.
Requires FlexDCA revision A.01.70 and above.
Measurement regions are only available in Oscilloscope and TDR modes.
Example Command Sequence
:SYSTem:MODE OSCilloscope :MEASure:REGions:COUNt 1 :MEASure:REGions:REGion1:X1 40E-12 :MEASure:REGions:REGion1:X2 100E-12 :MEASure:REGions:STATe ON