Threshold Configuration
Meas. mode:
Scope
Eye
TDR
Flex Apps:
FlexDCA
FlexRT
In Oscilloscope and Eye/Mask Modes, the threshold commands allow you to specify the upper, middle, and lower waveform threshold values. Waveform threshold levels can be set to standard percentages or to user-definited levels based on absolute amplitudes using the :MEASure:THReshold:METHod command. Custom values are specified, depending on waveform source, by the commands listed in the following table.
| Level | Levels Based On | |
|---|---|---|
| Percentage | Unit Amplitude | |
| Upper Level | :MEASure:THReshold:DISTal | :CHANnel:UDEFined:DISTal
:DIFF:UNDEFined:DISTal :EMEMory:UDEFined:DISTal :WMEMory:UDEFined:DISTal :FUNCtion:UDEFined:DISTal |
| Middle Level | :MEASure:THReshold:MESial | :CHANnel:UDEFined:MESial
:DIFF:UNDEFined:MESial :EMEMory:UDEFined:MESial :WMEMory:UDEFined:MESial :FUNCtion:UDEFined:MESial |
| Lower Level | :MEASure:THReshold:PROXimal | :CHANnel:UDEFined:PROXimal
:DIFF:UNDEFined:PROXimal :EMEMory:UDEFined:PROXimal :WMEMory:UDEFined:PROXimal :FUNCtion:UDEFined:PROXimal |