:MEASure:JITTer:DEFine:LEVel:CUSTom
Command:
Deprecated
Deprecated command. For FlexDCA revision A.05.60 and above, use the :MEASure:JITTer:DEFine:LEVel:CUSTom:EYE command instead.
Command Syntax
:MEASure:JITTer:DEFine:LEVel:CUSTom <amplitude>
<amplitude> is a double.
Query Syntax
:MEASure:JITTer:DEFine:LEVel:CUSTom?
Description
Sets the jiter sampling level (Watts or volts based on the optical or electrical input channel used) when the sampling level is specified to be units (:MEASure:JLTYpe command).
Requires Jitter Mode license.
Example Command Sequence
:MEASure:JITTer:DEFine:LEVel:TYPe UNITs :MEASure:JITTer:DEFine:LEVel:CUSTom 4.0E-04