:MEASure:JITTer:DEFine:LEVel:PERCent
Command:
Deprecated
Deprecated command. For FlexDCA revision A.05.60 and above, use the :MEASure:JITTer:DEFine:LEVel:PERCent:EYE command instead.
Command Syntax
:MEASure:JITTer:DEFine:LEVel:PERCent <percent>
<percent> is a double.
Query Syntax
:MEASure:JITTer:DEFine:LEVel:PERCent?
Description
Sets the pecentage level when the jiter sampling level is set to percent. Set the level between 30% and 70% of the eye amplitude. Use the :MEASure:JLTYpe command to change the type of sampling level to percent.
Requires Jitter Mode license.
Example Command Sequence
:MEASure:JITTer:DEFine:LEVel:TYPe PERCent :MEASure:JITTer:DEFine:LEVel:PERCent 5.0E+01