:RDCA:CONNect:METHod
Instrument:
N1000A
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
FlexPLL
Command Syntax
:RDCA:CONNect:METhod {LAN | USB | GPIB}
Query Syntax
:RDCA:CONNect:METhod?
Description
Establishes the method used to create a connection to an N1000A instrument. The Factory Preset setting is LAN.
- LAN
- Specifies a LAN connection. Use the
:RDCA:CONNect:HOSTcommand to enter the actual host ID of the N1000A. - USB
-
Specifies a USB connection. Use the
:RDCA:CONNect:USB:SADDresscommand to query or specify the USB address of the N1000A. When you connect the USB cable, FlexDCA automatically discovers the DCA-X on USB. Use a USB 3.0 type A to Type B cable where the Type B plug is connected to the DCA-X's rear-panel Type B receptical which is shown in the following picture.
Do not connect the USB cable to the N1000A's rear panel USB Type A receptical. The USB connection only works if the cable is connected to the USB Type B device-side receptical.
Requires FlexDCA revision A.06.40 and above for connections via USB.
- GPIB
- Specifies a GPIB connection. Use the
:RDCA:CONNect:GPIB:INAMecommand to specify the GPIB interface address and the:RDCA:CONNect:GPIB:ADDResscommand to enter the actual address of the N1000A.