:RDCA:CONNect:STATe?
Instrument:
N1000A
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
FlexPLL
Query Syntax
:RDCA:CONNEct:STATe?
Description
Queries the state of the connection between FlexDCA and an N1000A. Returns one of the following strings:
CONN- A flex-on-flex connection is established to an N1000A.
NCON- A connection is not established.
TOUT- A flex-on-flex connection to an N1000A has timed out.