:RDCA:DISConnect:TSETtings
Instrument:
N1000A
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
FlexPLL
Command Syntax
:RDCA:DISConnect:TSETtings {ON | OFF | 1 | 0}
Query Syntax
:RDCA:DISConnect:TSETtings?
Description
Sets or clears the Push State to Instrument on Disconnect setting on the FlexDCA Connection Setup dialog. This option determines what happens immediately before disconnecting the PC's N1010A FlexDCA from the FlexDCA on an N1000A. When selected, the instrument state of the PC's N1010A FlexDCA is copied to the FlexDCA on the N1000A. The display and settings on the N1000A's FlexDCA will match the display and settings that were on the PC's N1010A FlexDCA.
To set or clear the Pull State from Instrument on Connect setting, use the :RDCA:CONNect:TSETtings command. Use the :RDCA:CONNect command followed by an *OPC? query to actually make the connection.
Requires FlexDCA revision A.05.30 and above.