:RDCA:CONNect:TSETtings
Instrument:
N1000A
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:RDCA:CONNect:TSETtings {ON | OFF | 1 | 0}
Query Syntax
:RDCA:CONNect:TSETtings?
Description
Sets or clears the Pull State from Instrument on Connect setting on the FlexDCA Connection Setup dialog. This option determines what happens immediately after the connection is made between the PC's N1010A FlexDCA and the FlexDCA on an N1000A. When selected, the instrument state of the N1000A's FlexDCA is copied to the PC's N1010A FlexDCA. The display and settings on the PC's FlexDCA will match the display and settings that were on the N1000A's FlexDCA.
To set or clear the Push State to Instrument on Disconnect setting, use the :RDCA:DISConnect:TSETtings command. Use the :RDCA:CONNect command followed by an *OPC? query to actually make the connection.
Requires FlexDCA revision A.05.30 and above.