:SPRocess:FFEQualizer:TSPacing:TPBit

Command:
Deprecated

Deprecated command. For FlexDCA revision A.05.60 and above, use the :SPRocess:FFEQualizer:TSPacing:TPUI command.

Command Syntax

:SPRocessN:FFEQualizer:TSPacing:TPBit <number>

<number> is an integer.

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Description

Specifies tap spacing in taps-per-bit for a Linear Equalizer operator (:FUNCtion:FOPerator FFEQualizer). To select tap spacing in seconds or taps-per-bit, use the :SPRocess:FFEQualizer:TSPacing command. This command is available in both automatic and manual tap configuration mode.

Beginning with FlexDCA revision A.05.60, use of an *OPC? query to pause program execution while waiting for this command to execute.

The Linear Feedforward Equalizer operator is provided with the N1010A-201 Advanced Waveform Analysis license.

Example Command Sequence

:FUNCtion2:FOPerator FFEQualizer
:SPRocess2:FFEQualizer:TAPS:AUTo ON;*OPC?
:SPRocess2:FFEQualizer:TAPS:COUNt 5;*OPC?
:SPRocess2:FFEQualizer:NPRecursors 3;*OPC?
:SPRocess2:FFEQualizer:TSPacing:TPBit 2;*OPC?
:SPRocess2:FFEQualizer:BANDwidth:AUTo OFF
:SPRocess2:FFEQualizer:BANDwidth 8.0E9
:FUNCtion2:COLor TCOLor4
:FUNCtion2:DISPlay ON
*OPC?
…  //  Your code to synchronize execution timing.