:SPRocess Subsystem
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Package License:
L-RND
Use the :SPRocess subsystem to configure a Waveform Signal Processing operator's unique attributes. Use the :FUNCtion subsystem to:
- Create a Waveform Signal Processing operator,
- Assign a function number for the operator,
- Specify input waveforms and tracking, and
- Apply output waveform colors and scaling.
The following figure shows a typical setup dialog for an operator.
Operators are identified by their function assignment number (1 through 64) which is included in the SPRocess{1:64} command. The following figure shows a Gaussian operator assigned to Function 1. Commands in this subsystem allow you to select the Gaussian operator's filter cutoff frequency. Before configuring an operator, assign the operator to a function using the :FUNCtion:FOPerator command in the :FUNCtion subsystem.
To create and configure a function:
- Use the
:FUNCtion:FOPeratorcommand (:FUNCtion subsystem) to create the function. - Use the commands in the
:SPRocesssubsystem to configure your function.