:SPRocess:CTLequalizer:PCOunt
Command:
Deprecated
Deprecated command. For FlexDCA revision A.06.60 and above, use the :SPRocess:CTLequalizer:DEFinition command.
Command Syntax
:SPRocessN:CTLequalizer:PCOunt {2 | 3}
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Syntax
:SPRocessN:CTLequalizer:PCOunt?
Description
Specifies the number of poles for a Continuous Time Linear Equalizer (CTLE) operator (:FUNCtion:FOPerator CTLE). The query form of the command returns the number of poles.
Requires FlexDCA revision A.05.50 and above.