:SPRocess:RANDom:JITTer
Command:
Deprecated
Deprecated command. For FlexDCA revision A.06.60 and above, use the :SPRocess:RANDom:JITTer:RMS command.
Command Syntax
:SPRocessN:RANDom:JITTer <jitter>
<jitter> is a double.
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Syntax
:SPRocessN:RANDom:JITTer?
Description
Specifies the amount of jitter, in seconds, applied by a Random operator (:FUNCtion:FOPerator RANDom).