:TIMebase:BRANge
Command:
Deprecated
Deprecated command. For FlexDCA revision A.05.60 and above, use the :TIMebase:UIRange command.
Command Syntax
:TIMebase:BRANge <bits>
<bits> is a double.
Query Syntax
:TIMebase:BRANge?
Description
Sets the number of bits displayed across the graticule's horizontal axis, when the timebase units are set to bits (:TIMebase:UNITs). Use :TIMebase:BPOSition to set the bit delay. Use :TIMebase:BRATe to automatically set the bits displayed and bit delay based on the bit rate.
In Jitter Mode, bit rate, bits displayed, and bit delay controls are disabled. Do not use this command in Jitter Mode. It generates an error.
Example Command Sequence
:TIMebase:UNITs BIT :TIMebase:BRANge 5.0E-01 :TIMebase:BPOSition 2.39874E+02