:TIMebase:UIRange
Instrument
N1000A
N109x
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter
Command Syntax
:TIMebase:UIRange <unit intervals>
<unit intervals> is a double.
Query Syntax
:TIMebase:UIRange?
Description
Sets the number of Unit Intervals (UIs) displayed across the graticule's horizontal axis, when the timebase units are set to UIs (:TIMebase:UNITs). Use :TIMebase:UIPosition to set the UI delay. Use :TIMebase:SRATe to automatically set the symbols displayed and UI delay based on the symbol rate.
In Jitter Mode, symbol rate, symbols displayed, and symbol delay controls are disabled. Do not use this command in Jitter Mode. It generates an error.
Requires FlexDCA revision A.05.60 and above.
This command replaces deprecated command :TIMebase:BRANge.
Common Numerical Child Commands
This command supports the use of the following common numerical child commands: :DEFault, :MAXimum, :MINimum, and :STEP.
Example Command Sequence
:TIMebase:UNITs UINTerval :TIMebase:UIRange 5.0E-01 :TIMebase:UIPosition 2.39874E+02