:TIMebase:FIND:SIGNal
Command Syntax
:TIMebase:FIND:SIGNal CHANN
Where N identifies a specific channel and must be selected from {1:8}{A|B|C|D}. For example, 3C.
Query Syntax
:TIMebase:FIND:SIGNal?
Description
Selects a pattern waveform on which to perform a symbol sequence search. Use the :TIMebase:FIND:SEQuence command to define the specific sequence of symbols to search for within the pattern. Use the :TIMebase:FIND:NEXT command to initiate the search. Each use ot the NEXT command locates the next location in the pattern that matches the sequence.
To use this feature, pattern lock must be turned on (:TRIGger:PLOCk). It is recommended that the entire pattern be acquired (:ACQuire:EPATtern) and that waveform wrapping be turned off (:ACQuire:WRAPping).
Requires FlexDCA revision A.01.80 and above.
The Find Bit Sequence feature is available in Oscilloscope and Eye/Mask modes only.
Example
:TIMebase:FIND:SIGNal CHAN1A