:TIMebase:FIND:NEXT
Command Syntax
:TIMebase:FIND:NEXT
Description
Locates the next location of a symbol sequence within a waveform pattern as defined by the :TIMebase:FIND:SEQuence command. Use the :TIMebase:FIND:SIGNal command to select the waveform on which to perform the search. Each use ot the NEXT command locates the next location in the pattern that matches the sequence. The time scale is automatically adjusted to zoom in on the symbol sequence. To query the symbol offset of a located symbol sequence within the pattern, use the :TIMebase:BPOSition query. The location of the sequence within the pattern is also shown in the Pattern Navigation Display that is located at the top of the FlexDCA's display.
To use this feature, pattern lock must be turned on (:TRIGger:PLOCk). It is recommended that the entire pattern be acquired (:ACQuire:EPATtern) and that waveform wrapping be turned off (:ACQuire:WRAPping).
Requires FlexDCA revision A.01.80 and above.
The Find Bit Sequence feature is available in Oscilloscope and Eye/Mask modes only.
Example
:TIMebase:FIND:NEXT