:TRIGger:BRATe:AUTodetect
Command:
Deprecated
Deprecated command. For FlexDCA revision A.05.60 and above, use the :TRIGger:SRATe:AUTodetect command.
Command Syntax
:TRIGger:BRATe:AUTodetect {ON | OFF | 1 | 0}
Query Syntax
:TRIGger:BRATe:AUTodetect?
Query Response
{1 | 0}
Description
Enables or disables automatic symbol-rate detection. When turned off, use the :TRIGger:BRATe command to set the symbol rate. When turned on, send the :TRIGger:PLOCk ON or :SYSTem:PAUTodetect command to actually detect the symbol rate.
Example Command Sequence
:TRIGger:BRATe:AUTodetect ON :TRIGger:PLOCk ON