:TRIGger:PALign
Command:
Deprecated
Deprecated command. For FlexDCA revision A.06.71 and above, use the :TRIGger:RSYMbol:AUTodetect command.
Command Syntax
:TRIGger:PALign {ON | OFF | 1 | 0}
Query Syntax
:TRIGger:PALign?
Description
Automatically determines the reference symbol for the pattern and aligns the timebase with the reference symbol. The location is selected based on the longest run of symbols with a preference for lowest-level symbols. The pattern at the reference symbol is aligned to the display's left edge. To realign the timebase to use the left edge of the screen as the reference symbol for the pattern use the :TRIGger:SRSYmbol command.
This feature is only available in Scope mode.
Requires FlexDCA revision A.06.50 and above.