:TRIGger Subsystem
Send the Trigger (:TRIGger) subsystem commands to configure standard and pattern lock triggering for data acquisition. The commands are listed in three navigation panels in this topic: General Trigger, Advanced Trigger, and Pattern Lock commands.
General Trigger Commands (Trigger Setup dialog)
Use to configure an N1000A DCA-X and DCA-M oscilloscope settings in the General Trigger Setup tab. This includes trigger source, trigger level, and pattern locking.
Advanced Trigger Commands (Trigger Setup dialog)
Use to configure an N1000A DCA-X and DCA-M oscilloscope settings in the Advanced Trigger Setup tab. This includes waveform slope (hysteresis) and pattern locking when using the Rapid Eye feature. To use these settings, you must first turn pattern lock off.
Pattern Lock Commands (Trigger Setup dialog)
Use to configure an N1000A DCA-X settings in the Pattern Lock Setup tab.
:TRIGger:SOURce:AUTodetect ON :TRIGger:PLOCk ON;*OPC? :SYSTem:PAUTodetect
The information on triggering and pattern lock does not apply when FlexRT is enabled in FlexDCA. Triggering and pattern lock is not needed or used in FlexRT.
N109x (Slot X) Trigger Commands (Trigger Setup dialog)
When a DCA-M oscilloscope is installed, the Trigger Setup dialog includes a N109x (Slot X) Trigger tab that includes pattern lock settings like those in the Pattern Lock tab. To configure the DCA-M's pattern lock settings, use the commands found in the :SLOT subsystem.
If you turn the DCA-M's Shared Pattern Parameters setting on (:SLOT:TRIGger:TRACKing command), all settings in the Pattern Lock tab will automatically set and configure the settings in the N109x (Slot X) Trigger tab. If you use multiple DCA-Ms, this feature allows you to quickly set all pattern locking to the same settings.
Required Trigger Signal
A trigger signal must be provided to the oscilloscope using one of the following methods:
If you are using an 86107A Precision Timebase module and the time reference is set, all external trigger sources and controls are disabled.
1. On a DCA-X oscilloscopes
The easiest method is to connect a synchronous clock signal to the N1000A's front-panel Trigger connector. Use automatic trigger source detection which is the default triggering:
:TRIGger:SOURce:AUTodetect ON # default setting
Or, connect a synchronous clock signal, turn automatic trigger source detection off, and use the following command and argument to explicitly select Front Panel triggering:
:TRIGger:SOURce:AUTodetect OFF :TRIGger:SOURce FPANel :SYSTem:AUToscale # Sets trigger level to amplitude midpoint
With automatic trigger source detection off, you can manually set the trigger level:
:TRIGger:SOURce:AUTodetect OFF :TRIGger:SOURce FPANel :TRIGger:MODe EDGE # edge triggering :TRIGger:LEVel 30E-3 # trigger level
2. On a DCA-M oscilloscope
The easiest method is to connect a synchronous clock signal to the DCA-M's Clock Trigger In connector. Use automatic trigger source detection which is the default triggering:
:TRIGger:SOURce:AUTodetect ON # default setting
Or, connect a synchronous clock signal, turn automatic trigger source detection off, and use the following command and argument to explicitly select Front Panel triggering:
:TRIGger:SOURce:AUTodetect OFF :TRIGger:SOURce FPANel :SYSTem:AUToscale # Sets trigger level to amplitude midpoint
With automatic trigger source detection off, you can manually set the trigger level:
:TRIGger:SOURce:AUTodetect OFF :TRIGger:SOURce FPANel :TRIGger:MODe EDGE # edge triggering :TRIGger:LEVel 30E-3 # trigger level
3. Unavailable Trigger Signal
Use one of these three methods:
- If the DCA-X module or DCA-M has clock recovery, use clock recovery to recover the clock. Compatible modules include N1060A, 86108A/B, and N1092A/B series DCA-M modules. Use the following command and argument to select clock triggering:
:TRIGger:SOURce:AUTodetect OFF :TRIGger:SOURce CLOCk
:TRIGger:SOURce:AUTodetect OFF :TRIGger:SOURce FPANel
:TRIGger:SOURce:AUTodetect OFF :TRIGger:SOURce FRUN # free run triggering