:TRIGger:SRSYmbol
Command:
Deprecated
Deprecated command. For FlexDCA revision A.06.71 and above, use the :TRIGer:RSYMbol:SCTimebase command.
Command Syntax
:TRIGger:SRSYmbol
Description
Realigns the timebase to use the left edge of the screen as the reference symbol for the pattern. You can first position a symbol at the screen's left edge using one of the following two methods:
- Use the Find symbol sequence dialog. In FlexDCA's menu, click Tools > Find.... Or, use the
:TIMebase:Find:Sequenceand:TIMebase:FIND:NEXTcommands as show here:
:TIMebase:FIND:SEQuence "1101" :TIMebase:FIND:NEXT
:TIMebase:UNITs and :TIMebase:UIRPosition commands.:TIMebase:UNITs UINTerval :TIMebase:UIRPosition 8.8E+1
To automatically determine the reference symbol for the pattern and align the timebase with the reference symbol use the :TRIGger:PALign command.
This feature is only available in Scope mode.
Requires FlexDCA revision A.06.50 and above.