:TRIGger:BRATe
Command:
Deprecated
Deprecated command. For FlexDCA revision A.05.60 and above, use the :TRIGger:SRATe command.
Command Syntax
:TRIGger:BRATe <rate>
<rate> is a double.
Query Syntax
:TRIGger:BRATe?
Description
When using pattern lock, use this command to enter or read the symbol-rate of the trigger source. Automatic detection must be turned off before the entered symbol rate setting is applied (:TRIGger:BRATe:AUTodetect).
Example Command Sequence
:TRIGger:BRATe:AUTodetect OFF :TRIGger:BRATe 2.0E+10