:TRIGger:LEVel
Instrument
N1000A
N109X
Flex Apps:
FlexDCA
Command Syntax
:TRIGger:LEVel <level>
<level> is a double.
Query Syntax
:TRIGger:LEVel?
Description
Specifies the trigger level on all trigger inputs. This is the threshold level that the trigger signal must cross to trigger on the signal. You can enter a level between −1.0V and 1.0V. The trigger level can be adjusted whenever the trigger bandwidth (:TRIGger:MODE) is set to Filtered (FILTered) or Edge (EDGE. When the trigger bandwidth setting is set to CLOCk, the trigger level is AC coupled and cannot be manually adjusted. The level that you select for the trigger threshold is applied to all trigger sources.