:TRIGger:MODe
Command Syntax
:TRIGger:MODe {FILTered | EDGE | CLOCk}
Query Syntax
:TRIGger:MODe?
Description
When the trigger source is set to the front panel (:TRIGger:SOURce FPANel) and pattern lock is turned off (:TRIGger:PLOCk OFF), selects the trigger mode in Oscilloscope mode and Eye/Mask mode:
- FILTered
- Selects Filtered Edge (DC to 100 MHz) trigger bandwidth. You can set the trigger level using the
:TRIGger:LEVelcommand. - EDGE
- Selects Standard Edge (DC to 3.2 GHz) trigger bandwidth.
- CLOCk
- Selects Clock/Divided (3 GHz to 13 GHz) trigger bandwidth.
The trigger signal's sensitivity to noise and response time is affected by the bandwidth. Selection of the proper mode (bandwidth) is a compromise between the trigger's response to very fast edge speeds and its sensitivity to noise. Noise on the trigger signal can result in inconsistent triggering, which is seen as timing instability (jitter) in the displayed waveform. To reduce the occurrence of inconsistent triggering, reduce the bandwidth of the trigger circuitry. When pattern lock is turned on, triggering information is automatically detected as the FlexDCA generates a pattern lock. In this case, trigger bandwidth settings are not used and are unavailable.
Requires FlexDCA revision A.03.00 and above.
Example Command Sequence
:SYSTem:MODE EYE :TRIGger:SOURce FPANel :TRIGger:PLOCk OFF :TRIGger:MODE CLOCk