:TRIGger:SOURce
Instrument
N1000A
N109X
Flex Apps:
FlexDCA
Command Syntax
:TRIGger:SOURce {FRUN | FPANel | CHANnel{1:8}{A|B|C|D} | SLOT{1:4}}
Where the {1:8}{A|B|C|D} specifier identifies a channel. For example, CHANnel3C.
Where the {1:4} specifier identifies a module slot.
Query Syntax
:TRIGger:SOURce?
Description
Selects the trigger input for the N1000A and DCA-M products like the N1090A and N1090A/B/D optical sampling oscilloscopes. The following sources can be selected:
- FRUN
- Free Run. Triggers the data acquisition as soon as the trigger is armed, without having to provide an external trigger. Free run is asynchronous to the data. Use free-run triggering as an easy way to examine the amplitude of a signal without any timing information.
- FPANel (default setting)
- Front Panel. Triggers the data acquisition from an external trigger source that is connected to the front-panel Trigger input. This is the most often-used method (as well as the default) source for triggering. Use the
:TRIGger:LEVelcommand to set the trigger level, when the trigger bandwidth (:TRIGger:MODE) is set toFILTeredorEDGe. - CHANnel{1:8}{A|B|C|D}
- Channel. Trigger from a channel. This selection is not available for DCA-M products.
- SLOT{1:4}
- Module Slot. Trigger from a plug-in module slot location (1 through 4). Compatible modules (that have front-panel trigger input connectors) include 86108A (always SLOT1) and 8349x-series (SLOT1 or SLOT3). When an 86108A precision waveform analyzer module is installed, triggering can be from the recovered clock or from the precision timebase. When using the 86107A Precision Timebase module and the time reference is set, all external trigger sources and controls are disabled. This selection is not available for DCA-M products.
Example Command Sequence
:TRIGger:SOURce FPANel :TRIGger:MODE CLOCk :SYSTem:MODE EYE