:WAVeform:EYE:POINts?
Instrument:
N1000A
DCA-M
Meas. mode:
Eye
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:WAVeform:EYE:POINts?
Description
Returns the number of points in the color grade/gray scale data array, which is always 391,271. Use the :WAVeform:EYE:ASCii:DATa? or :WAVeform:EYE:INTeger:DATa? queries to actually transfer the array. The data is transferred as a two dimensional array consisting of 521 rows by 751 columns for a total number of 391,271 points. This array corresponds to the graticule display, where each point is a sample hit count. The array is transferred column by column, starting with the lower left corner of the graticule.
Requires Eye/Mask Mode (:SYSTem:MODE).