:WAVeform:EYE:STATus?
Instrument:
N1000A
DCA-M
Meas. mode:
Eye
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:WAVeform:EYE:STATus?
Description
Queries the status of the color-grade gray-scale waveform data and returns the strings shown in the following table. Use the :REASon child query to return a string that indicates why the data is invalid or questionable.
| Response | Description |
|---|---|
| CORR | The waveform data is correct. |
| INV | The waveform data is invalid. Check to see if eye diagram data is displayed on the screen. |
| QUES | The waveform data is questionable. Confirm that the eye diagram data is not clipped high, clipped low, or has holes. |
Query the data using one of the following two commands:
Requires FlexDCA revision A.03.00 and above.