:WAVeform:EYE:STATus:REASon?
Instrument:
N1000A
DCA-M
Meas. mode:
Eye
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:WAVeform:EYE:STATus:REASon?
Description
Queries a string that explains why the :STATus parent command indicates invalid or questionable waveform data. The following strings may be returned by this query:
- ""
- A null string indicates that the data is correct.
- "Clipped Hi"
- The amplitude of the waveform is too large and the data is clipped off the top of the screen.
- "Clipped Low"
- The amplitude of the waveform is too large and the data is clipped off the bottom of the screen.
Requires FlexDCA revision A.03.00 and above.