:WAVeform:XYFormat:POINts?
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:WAVeform:XYFormat:POINts?
Description
Queries the record length (number of points) in the waveform's XYFormat data. Use :WAVeform:SOURce to select the source waveform. Use the :CLIPped:HIGH?, :CLIPped:LOW?, and :HOLes? child queries to return a list of points that have clipped or missing data (holes). On a waveform acquisition, data can be missing in one of the following situations:
- When a precision timebase is used, occasionally data may be missing on a few points.
- When an entire waveform pattern is being acquired and the acquisition has not yet completed.