:WAVeform:XYFormat:POINts:CLIPped?
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:WAVeform:XYFormat:POINts:CLIPped?
Description
Queries the number of points in the waveform's XYFORmat data that are clipped, which includes points that are clipped high or clipped low. The amplitude of a clipped-high data point is too high to be displayed on the screen. The amplitude of a clipped-low data point is too low to be displayed on the screen. Clipped-high and clipped-low data points have the value NaN (9.91E+37). Use the :SYSTem:AUToscale command to properly scale the waveform to the display. Use :WAVeform:SOURce to select the source waveform. Use the :HIGH and :LOW child commands to determine how number of points that are either clipped high or low.
Requires FlexDCA revision A.03.00 and above.