:WMEMory:FILE:NAME
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Waveform type:
NRZ
PAM4
Command Syntax
:WMEMory{1:8}:FILE:NAME "filename"
Where the {1:8} specifier identifies one of eight possible waveform memories. For example, :WMEMory4.
Query Syntax
:WMEMory{1:8}:FILE:NAME?
Query Response
"string"
Description
Enters the name (including path) of a file to be imported into an waveform memory using the :WMEMory:FILE:LOAD command. If no path is given, the file expected to be in the default \Waveforms folder.
Requires FlexDCA revision A.05.70 and above.