:WMEMory:LOAD
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Waveform type:
NRZ
PAM4
Command Syntax
:WMEMory{1:8}:LOAD
Where the {1:8} specifier identifies one of eight possible waveform memories. For example, :WMEMory4.
Description
Loads the selected waveform source into the indicated waveform-memory location. Use the :WMEMory:LOAD:SOURce command to select the source. Use the :WMEMory:DISPLay command to display the waveform-memory.
To load a waveform file into waveform memory, use the :WMEMory:FILE:LOAD and :WMEMory:FILE:SOURce commands.
Example Command Sequence
:WMEMory2:LOAD:SOURce CHAN1A :WMEMory2:LOAD :WMEMory2:DISPLay ON
Child Commands
:SOURcespecifies the source waveform on which to perform the measurement.