:WMEMory:LOAD:SOURce
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Waveform type:
NRZ
PAM4
Command Syntax
:WMEMory{1:8}:LOAD:SOURce <source_waveform>
Where the {1:8} specifier identifies one of eight possible waveform memories. For example, :WMEMory4.
Where <source_waveform> can be one of the following:
CHANnel{1:8}{A|B|C|D}DIFF{1:4}CGMemory{1:8}FUNCtion{1:16}
Query Syntax
:WMEMory{1:8}:LOAD:SOURce?
Description
Selects the source waveform to load into waveform memory. Use the :WMEMory:LOAD command to actually load the selected source.
Example Command Sequence
:WMEMory2:LOAD:SOURce CHAN3A :WMEMory2:LOAD