:WMEMory:UDEFined:PROXimal
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Waveform type:
NRZ
PAM4
Command Syntax
:WMEMory{1:8}:UDEFined:PROXimal amplitude
<amplitude> is a double.
Where the {1:8} specifier identifies one of eight possible waveform memories. For example, :WMEMory4.
Query Syntax
:WMEMory{1:8}:UDEFined:PROXimal?
Description
Sets the lower threshold definition level. This value is used when making measurements with custom threshold definitions that are based on absolute amplitude. When custom threshold definitions are based on percent, use the :MEASure:THReshold:PROXimal command.
Use the :MEASure:THReshold:METHod command to specify the use of custom threshold definitions. Use the :MEASure:THReshold:UNITs command to select levels base on absolute amplitude values.
Use the :WMEMory{1:8}:UDEFined:DISTal command to enter a upper threshold level. Use the :WMEMory{1:8}:UDEFined:MESial command to enter a middle threshold level.
Example Command Sequence
:MEASure:THReshold:METHod UDEFined :MEASure:THReshold:UNITs UNITs :MEASure:UTSRc CHANnel1 :WMEMory4:UDEFined:DISTal 125E-3 :WMEMory4:UDEFined:MESial 0E0 :WMEMory4:UDEFined:PROXimal -125E-3