:WMEMory:UDEFined:DISTal
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Waveform type:
NRZ
PAM4
Command Syntax
:WMEMory{1:8}:UDEFined:DISTal amplitude
<amplitude> is a double.
Where the {1:8} specifier identifies one of eight possible waveform memories. For example, :WMEMory4.
Query Syntax
:WMEMory{1:8}:UDEFined:DISTal?
Description
Sets the upper threshold-definition level. This value is used when making measurements with custom threshold definitions that are based on absolute amplitude. When custom threshold definitions are based on percent, use the :MEASure:THReshold:DISTal command.
Use the :MEASure:THReshold:METHod command to specify the use of custom threshold definitions. Use the :MEASure:THReshold:UNITs command to select levels base on absolute amplitude values.
Use the :WMEMory{1:8}:UDEFined:MESial command to enter a middle threshold level. Use the :WMEMory{1:8}:UDEFined:PROXimal command to enter a lower threshold level.
Example Command Sequence
:MEASure:THReshold:METHod UDEFined :MEASure:THReshold:UNITs UNITs :MEASure:UTSRc CHANnel1 :WMEMory2:UDEFined:DISTal 125E-3 :WMEMory2:UDEFined:MESial 0E0 :WMEMory2:UDEFined:PROXimal -125E-3